INPut:TYPe <char>

(Read-Write) Set and query the USB or LAN power sensor type.

See also, INP:LAN:ADDR, INP:LAN:ID:TYP, INP:LAN:ID:SNUM, DISP:MOD:STAT,  INP:LAN:ID:NAME, and DISP:MOD:DATA.

Learn more, the FieldFox Supplemental Help.

Relevant Modes

Frequency Offset mode (Option 208), Power Meter mode (Option 310), and Pulse Measurements mode (Option 330)

Parameters

 

<char>

Choose from:

USB- Defines the sensor type as USB.

LAN- Defines the sensor type as LAN.

Examples

INP:TYP USB 'Defines the sensor type as USB

INP:TYP LAN 'Defines the sensor type as LAN

Query Syntax

INPut:TYPe?

Return Type

Character

Default

USB

Last Modified:

29july2019

New command (11.26)