DISPlay:MODel:STATe <char>

(Read-Write) Enable/disable the model annotations.

See also, INP:TYP, INP:LAN:ADDR, INP:LAN:ID:SNUM, INP:LAN:ID:TYP, INP:LAN:ID:NAME, and DISP:MOD:DATA.

Learn more, the FieldFox Supplemental Help.

Relevant Modes

Frequency Offset mode (Option 208), Power Meter mode (Option 310), and Pulse Measurements mode (Option 330)

Parameters

 

<char>

Choose from:

ON (1)- (default) the power sensor model annotations are displayed on the FieldFox.

OFF (0)- Disables the power sensor model annotations on the FieldFox.

Examples

DISP:MOD:STAT OFF 'Disable the model annotations

DISP:MOD:STAT 0'Disable the model annotations

Query Syntax

DISPlay:MODel:STATe?

Return Type

num

Default

1

Last Modified:

29july2019

New command (11.26)