(Read-Write) Set and query the LAN sensor's enumerator model and SCPI name. See also, INP:TYP, INP:LAN:ID:TYP, INP:LAN:ID:SNUM, DISP:MOD:STAT, INP:LAN:ADDR, and DISP:MOD:DATA. Learn more, the FieldFox Supplemental Help. |
|
Relevant Modes |
Frequency Offset mode (Option 208), Power Meter mode (Option 310), and Pulse Measurements mode (Option 330) |
Parameters |
|
<char> |
Choose a LAN sensor model number enumerator: Power Sensor Model: Enumerator: U2049XA UA1 L2061XA LA1 L2062XA LA2 L2063XA LA3 L2051XA LA4 L2052XA LA5 L2053XA LA6 L2054XA LA7 L2055XA LA8 L2064XA LA9 L2065XA LA10 L2065XT LT1 |
Examples |
INP:LAN:ID:NAM UA1 'Defines a model U2049XA LAN sensor INP:LAN:ID:NAM LA5 'Defines a model U2052XA LAN sensor |
Query Syntax |
INPut:LAN:ID:NAMe? |
Return Type |
character |
Default |
n/a (i.e., if no LAN sensor IP address is specified, the FieldFox returns "Not Specified". |
Last Modified:
01june2019 |
New command (11.26) |