INPut:LAN:ID:TYPe <char>

(Read-Write) Set and query the hostname.

See also, INP:TYP, INP:LAN:ADDR, INP:LAN:ID:SNUM, DISP:MOD:STAT,  INP:LAN:ID:NAME, and DISP:MOD:DATA.

Learn more, the FieldFox Supplemental Help.

Relevant Modes

Frequency Offset mode (Option 208), Power Meter mode (Option 310), and Pulse Measurements mode (Option 330)

Parameters

 

<char>

Choose from:

SNUM- (default) Uses the power sensor's serial number to automatically identify the power sensor.

IPA- Defines the sensor type as LAN.

Examples

INP:LAN:ID:TYP IPA 'Defines the IP address as the method to identify the hostname

Query Syntax

INPut:LAN:ID:TYP?

Return Type

char

Default

SNUM

Last Modified:

29july2019

New command (11.26)