(Read-Write) Set and query the LAN sensor's IP address. See also, INP:TYP, INP:LAN:ID:TYP, INP:LAN:ID:SNUM, DISP:MOD:STAT, INP:LAN:ID:NAME, and DISP:MOD:DATA. Learn more, the FieldFox Supplemental Help. |
|
Relevant Modes |
Frequency Offset mode (Option 208), Power Meter mode (Option 310), and Pulse Measurements mode (Option 330) |
Parameters |
|
<string> |
Enter an IP address for the LAN sensor. |
Examples |
INP:LAN:ADDR "111.111.111.111" 'Defines the IP address of the current LAN sensor |
Query Syntax |
INPut:LAN:ADDR? |
Return Type |
string |
Default |
n/a (i.e., if no LAN sensor IP address is specified, the FieldFox returns "Not Specified". |
Last Modified:
29july2019 |
New command (11.26) |