(Read-Write) Enable or disables the measurement interval. See also, DLOG:INT:TIME, DLOG:INT:DISTance, and DLOG:INT:TYPE. |
|
Relevant Modes |
Channel Scanner, 5G NR, 5G TF, 5G NR EVM Conducted, LTE FDD, Mapping, and PAA |
Parameters |
|
<bool> |
Choose from: Off or 0 - Disable the measurement interval On or 1 - Enable the measurement interval (1 km to 10 km) |
Examples |
:DLOGging:INTerval Off 'Disables the measurement interval :DLOGging:INTerval:ENABled 1 'Enables the measurement interval |
Query Syntax |
:DLOGging:INTerva? |
Return Type |
numeric |
Default |
0 (OFF) |
Last Modified:
01dec2020 |
Updated command (12.1x) |