(Read-Write) Sets the value of the distance interval. See also, DLOG:INT:TIME, DLOG:INT:TYPE, and DLOG:INT[:ENABled]. |
|
Relevant Modes |
Channel Scanner, 5G NR, 5G TF, 5G NR EVM Conducted, LTE FDD, Mapping, and PAA |
Parameters |
n/a |
Examples |
:DLOGging:INTerval:DISTance 5 'sets the Distance value to 5 m :DLOGging:INTerval:DISTance 4e3 'sets the Distance value to 4 km |
Query Syntax |
:DLOGging:INTerval:DISTance? |
Return Type |
numeric |
Default |
10.0m |
Last Modified:
01dec2020 |
Updated command (12.1x) |