:DLOGging:INTerval:TIMe

(Read-Write) Sets the time interval (1 to 3,600 seconds).

See also, DLOG:INT:DISTance, DLOG:INT:TYPE, and DLOG:INT[:ENABled].

Relevant Modes

Channel Scanner, 5G NR, 5G TF, 5G NR EVM Conducted, LTE FDD, Mapping, and PAA

Parameters

 

<val>

 

Examples

:DLOGging:INTerval:TIMe 5

Query Syntax

:DLOGging:INTerval:TIMe?

Return Type

numeric

Default

10s


Last Modified:

01dec2020

Updated command (12.1x)