:DLOGging:INTerval:TYPe

(Read-Write) Sets the interval (1 to 3,600 seconds).

See also, DLOG:INT:TIME, DLOG:INT:DISTance, and DLOG:INT[:ENABled].

Relevant Modes

Channel Scanner, 5G NR, 5G TF, 5G NR EVM Conducted, LTE FDD, Mapping, and PAA

Parameters

 
 

Choose from:

time - sets the measurement interval type to time.

dist - sets the measurement interval type to distance.

Examples

:DLOGging:INTerval:TYPe time

:DLOGging:INTerval:TYPe Dist

Query Syntax

:DLOGging:INTerval:TYPe?

Return Type

character

Default

Time


Last Modified:

01dec2020

Updated command (12.1x)