(Read-Write) When the CORR:ENR:MOD is set to Smart (Auto) and Auto Load ENR is enabled (ON == Default), upon connection of a Smart Noise Source, the ENR Data will be automatically loaded into the ENR Table. This overwrites any existing data in the ENR Table data. Enables the reloading of ENR data, when used with the CORR:ENR:NOIS:CONN SCPI. This action overwrites any existing data in the ENR table. If set to OFF, the ENR Table menu will not be modified and no data will be loaded into any ENR table automatically. See also, CORR:ENR:MOD, CORR:ENR:NOIS:CONN, CORR:TCOL, and CORR:ENR:NOIS:STAT. |
|
Relevant Modes |
|
Parameters |
|
<boolean> |
|
Examples |
CORR:ENR:AUTO ON */Sets the ENR to autoload the ENR data. CORR:ENR:AUTO 0 */Disables the ENR autoload for the ENR data. |
Query Syntax |
CORR:ENR:AUTO? |
Return Type |
ON (1) - ENR is Autoload enabled OFF (0) - ENR data Autoload is disabled |
Default |
ON (1) |
Last Modified:
06sept2022 |
Added: NF mode updates for smart source feature (A.12.5x) |