(Read-Write) Set and query the ENR mode state preference. . NOTE: 2) If noise source preference (CORR:ENR:MOD) is set to SPOT or TABLe, this SCPI will not control the noise source drive state. See also CORR:ENR:MOD, CORR:ENR:NOIS:CONN, CORR:TCOL, and CORR:ENR:AUTO. |
|
Relevant Modes |
|
Parameters |
|
<character> |
ENR mode. Choose from: NORMal - When noise source detected and CORR:ENR:MOD is set to SMARt, CORR:ENR:NOIS:STAT is set to NORMal (default setting), the application controls the noise source on/off automatically during measurement and calibration. ON - When this function is set to ON, the application turns on the noise source and no valid results are provided . OFF - When this function is set to OFF, the application turns off the noise source and no valid results are provided . |
Examples |
CORR:ENR:NOIS:STAT SMAR */Turns on the Smart source (default) |
Query Syntax |
CORRection:ENR:MODe? |
Return Type |
Character |
Default |
NORM |
Last Modified:
06sept2022 |
Added: NF mode updates for smart source feature (A.12.5x) |