[:SENSe]:CORRection:ENR:NOISe:CONNect

(Write-Only) Enables the User to attempt to connect to the USB Noise Source. This process is automatically controlled by the FieldFox, which takes about 10-20s. If this automatic detection fails, this softkey will enable the user to connect manually.

NOTE: When this command is used with the CORR:ENR:NOIS:CONN SCPI enables the reloading of ENR table data. This action overwrites the existing ENR table data.

See also, CORR:ENR:MOD, CORR:ENR:NOIS:STAT, CORR:TCOL, and CORR:ENR:AUTO.

Relevant Modes

NF

Parameters

n/a

   

Examples

CORR:ENR:NOISE:CONN */SCPI tells the instrument to check for a compatible noise source

Query Syntax

Not Applicable

Default

Not Applicable


Last Modified:

06sept2022

Added: NF mode updates for smart source feature (A.12.5x)