Write-only |
About Exporting Data |
Description |
Export data by specifying parameters with this method. You can also specify parameters using separate commands. Learn how. |
VB Syntax |
doc.ExportTimeDomainTextFile (fileName, delimiterType, dataFormat, portNmbr, portMap, diffPortMap, dutCfgDesc, dataToExport, paramList, ExportInOneFile, timeUnit, dataRange, startTimeNs, stopTimeNs, stepTimeNs |
Variable |
(Type) - Description |
|
doc |
(object) - A PLTSDoc object |
|
fileName |
(String) Full path, file name, and suffix of exported file. |
|
delimiterType |
(Integer) Choose the type of text file to export. 0 - Tab 1 - Comma |
|
dataFormat |
(Integer)(Enum as pltsFreqDomainTextFileDataFormat) Data format. Choose from: 0 - StepReal 1 - ImpulseReal 2 - StepVolts 3 - ImpulseVolts 4 - StepLog 5 - ImpulseLog 6 - StepImpedance Learn more about time domain format. |
|
portNmbr |
(Integer) - Number of DUT ports for which data will be exported. Learn more. -1 specifies the port number of the original data. |
|
portMap |
(String) Mapping of ports to export. Learn more " " specifies the original port mapping. |
|
diffPortMap |
(String) Mapping of ports to export. Learn more " " specifies the original port mapping. |
|
dutCfgDesc |
(String) Description of the DUT configuration after export. Learn more. Use " " to use the current DUT configuration. |
|
dataToExport |
(Enum as pltsTextFileDataToExport) Parameter data to export. Choose from: 0 - SE (all single-ended parameters) 1 - Balanced (all balanced parameters) 2 - All (all single-ended and balanced parameters) 3 - Customized (parameters selected using the following paramList argument. |
|
paramList |
(String) List of parameter to export separated by commas. Use " " when the previous argument is NOT Customized. Learn more. |
|
ExportInOneFile |
(Boolean) Export all data in one file or to separate files. Choose from: 0- False All selected parameters are saved to separate files. Each file is saved to the specified folder with the filename you entered and a parameter label appended to the name. For example, if you entered device4 as the file name, the S11 parameter file is named: device4_S11.txt. 1 - True All selected parameters are saved to one file. |
|
timeUnit |
(Enum as pltsTimeUnits) Units to use when exporting time domain data. Choose from: 0 - Ns (Nano seconds) 1 - Cm (centimeters) |
|
dataRange |
(Integer) The data range to export. Choose from: 0 - RangeAll - Export the entire data range in PLTS memory. 1 - Subset The data range is specified with the following arguments: startTime, stopTime, steptime |
|
startTimeNs |
(Double) Start time to export when Subset of data is selected. |
|
stopTimeNs |
(Double) Stop time to export when Subset of data is selected. |
|
stepTimeNs |
(Double) Step time (number of points) to export when Subset of data is selected. |
Return Type |
None |
Default |
None |
Examples |
doc.ExportTimeDomainTextFile "C:/PLTS/MyDut.dut", 0,1,-1," "," ","MyExportedData",3,"S11,S22",0,1,1,1,1.5,2.5,.1 |
C++ Syntax |
HRESULT ExportTimeDomainTextFile(BSTR fileName, SHORT delimiterType, SHORT dataFormat, SHORT portNmbr, BSTR portMap, BSTR diffPortMap, BSTR dutCfgDesc, SHORT dataToExport, BSTR paramList, VARIANT_BOOL exportInOneFile, SHORT timeUnit, SHORT dataRange, DOUBLE startTimeNs, DOUBLE stopTimeNs, DOUBLE stepTimeNs); |
Interface |
IPLTSDocument |