IMD Applications (Opt 087)


The Intermodulation Distortion (IMD) App is offered for both Amplifiers and Converters, and also can be viewed in both Swept IMD and IM Spectrum channels.

Learn all about the IMD App (Opt 087) in the following topics:

Concepts

How to Use ALL IMD Apps

Requirements for Opt 087 IMD App

PNA-X or PNA (N522x) with:

Note: N522x models require additional configuration and equipment. See Configure External Source and Combiner for IMD Apps.

See Also