Controls an IMD and IMDx calibration. These commands supplement the Guided Cal commands.
|
SENSe:CORRection:IMD | CALibration | METHod | LO | PCAL | MPRoduct | POWer | SENSor | CKIT |
Click on a keyword to view the command details.
CALC:CUSTom:DEFine - creates an IMD measurement.
See Also
Example - Create and Cal an IMD measurement
|
(Read-Write) Sets and returns the frequencies at which an IMD source power cal is performed. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
|
<char> |
Choose from: CENTer - Perform source power calibration at only the center frequencies, midway between the main tones. ALL - Perform source power calibration at all main tone frequencies. |
|
Examples |
SENS:CORR:IMD:CAL:FREQ ALL sense2:correction:imd:calibration:frequencies center |
|
Query Syntax |
SENSe<cnum>:CORRection:IMD:CALibration:FREQuencies? |
|
Return Type |
Character |
|
Default |
CENTer |
|
(Read-Write) Sets and returns the method by which the match-correction portion of an IMD calibration is performed. Learn more. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
|
<char> |
Choose from: MATCh - Performs a full 2-port cal for full match-correction. RESPonse - Performs only a response (normalization) cal instead of a full 2-port cal. |
|
Examples |
SENS:CORR:IMD:CAL:METH MATC sense2:correction:imd:calibration:method response |
|
Query Syntax |
SENSe<cnum>:CORRection:IMD:CALibration:METHod? |
|
Return Type |
Character |
|
Default |
MATCh |
|
(Read-Write) Sets and returns whether or not the LO power cal step is included in the cal steps when an IMDX cal is performed. Learn more. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
|
<n> |
LO Stage. Choose 1. |
|
<char> |
LO Power Cal state. Choose from: O or OFF - Skips over the LO Power Cal when calibrating. 1 or ON - Includes a step for LO Power Cal when calibrating |
|
Examples |
SENS:CORR:IMD:LO1:PCAL 0 sense2:correction:imd:lo1:pcal:state on |
|
Query Syntax |
SENSe<cnum>:CORRection:IMD:LO<n>:PCAL[:STATe]? |
|
Return Type |
Boolean |
|
Default |
PNA Rev. 9.1 and above: 0 or OFF Before Rev 9.1: 1 or ON |
|
(Read-Write) Sets and returns the maximum intermod product frequencies to be calibrated. All lower product frequencies are also calibrated. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
|
<char> |
Maximum IM products to calibrate. Choose from: 2 - second order products 3 - third order products 5 - fifth order products 7 - seventh order products 9 - ninth order products |
|
Examples |
SENS:CORR:IMD:MPR 5 sense2:correction:imd:mproduct 9 |
|
Query Syntax |
SENSe<cnum>::CORRection:IMD:MPRoduct? |
|
Return Type |
Numeric |
|
Default |
3 |
|
(Read-Write) Sets and returns the power level at which to perform the source power calibration using a power sensor. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
|
<num> |
Power level. Choose a value between the min and max power level of the PNA. |
|
Examples |
SENS:CORR:IMD:POW -5 sense2:correction:imd:power 5 |
|
Query Syntax |
SENSe<cnum>::CORRection:IMD:POWer? |
|
Return Type |
Numeric |
|
Default |
0 |
|
(Read-Write) Sets and returns the cal kit to be used for calibrating at the port 1 reference plane when the power sensor connector is different from the DUT port 1. This effectively removes the effects of an adapter that is used to connect the power sensor. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
|
<string> |
Cal Kit enclosed in quotes. First set the DUT connector for port 1 and the connector of the power sensor. Then use SENS:CORR:COLL:GUID:CKIT:PORT1:CAT? to return a list of valid cal kits. |
|
Examples |
SENS:CORR:IMD:SENS:CKIT "85052B" |
|
Query Syntax |
SENSe<cnum>::CORRection:IMD:SENSor:CKIT? |
|
Return Type |
String |
|
Default |
Depends on the specified connectors |
|
(Read-Write) Sets and returns the power sensor connector type which is used to perform the Source Power Cal portion of an IMD calibration. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
|
<string> |
Power sensor connector type. Use SENS:CORR:COLL:GUID:CONN:CAT? to return a list of valid connector types. Select "Ignored" to NOT compensate for the adapter. |
|
Examples |
SENS:CORR:IMD:SENS:CONN "APC 3.5 male" sense2:correction:imd:sensor:connector "Ignored" |
|
Query Syntax |
SENSe<cnum>::CORRection:IMD:SENSor:CONNector? |
|
Return Type |
String |
|
Default |
"Ignored" |
|
(Read-Write) Sets and returns whether to include the second order products in the calibration. These frequencies of these products can be far from the main tones. |
|
|
Parameters |
|
|
<cnum> |
Any existing channel number; if unspecified, value is set to 1. |
|
<bool> |
Choose from: ON (or 1) - Include 2nd order products OFF (or 0) - Do NOT include 2nd order products |
|
Examples |
SENS:CORR:IMD:SORD:INCL ON |
|
Query Syntax |
SENSe<cnum>::CORRection:IMD:SORDer:INCLude? |
|
Return Type |
Boolean |
|
Default |
OFF or 0 |