Only the Main and Fixtures Cal commands corresponding to the Spectrum Analyzer measurement class are documented here. All other commands are identical to the Cal commands for the Standard measurement class and can be accessed by clicking here or by clicking on the softtabs on the graphic below.
Click here to view links to Cal commands for all Measurement Classes.
| Main Tab Commands | |||
Softkey |
Sub-item | SCPI |
COM |
|
|
||
|
|||
| Src Power Correct | ON/OFF | SOURce:POWer:CORRection[:STATe] | |
| Interpolation | ON/OFF | SENSe:CORRection:INTerpolate[:STATe] | |
| Correction Methods... |
|
||
| Correction Properties... | None | ||
| Fixtures Tab Commands | |||
| Softkey | Sub-item | SCPI | COM |
| Apply Fixtures | ON/OFF | CALCulate:FSIMulator:STATe | |
| Power Comp... | Port N | ||
Change order of operations |
None |
||
2 and 4-port Extrapolate |
|||
| 2-Port Fixturing | |||
Port matching ON and OFF |
|||
Reverse ports |
|||
Sets Port Matching circuit model |
|||
Sets Port Matching 'S2P' file name |
|||
Sets Capacitance 'C' value |
|||
Sets Conductance 'G' value |
|||
Sets Inductance 'L' value |
|||
Sets Resistance 'R' value |
|||
De-embed ON and OFF |
|||
Sets De-embedding circuit model |
|||
Sets De-embedding 'S2P' file name |
|||
Port Impedance ON and OFF |
|||
Port Z Real |
|||
Port Z Imag |
|||
Port Z Real and Imag |
|||
| Remote ONLY | |||
Create Cal Set with De-embeded fixture removed |
|||
Create Cal Set with Matching network included |
|||