:CALibrate:CALibrator:AOENable

Command Syntax

:CALibrate:CALibrator:AOENable {{OFF | 0} | {ON | 1}}

Query Syntax

:CALibrate:CALibrator:AOENable?

Description

This command enables or disables the calibrator output signal to appear on the AUX Out connector.

In the DC level calibrator mode (see :CALibrate:CALibrator:MODE), the output signal cannot be enabled on the AUX Out connector. However, this option is available for most AC modes.

Query Response

{0 | 1}