:CALibrate:CALibrator:FREQuency
Command Syntax
:CALibrate:CALibrator:FREQuency <Hz>
<Hz> is a double.
Query Syntax
:CALibrate:CALibrator:FREQuency?
Description
When the Frequency Synth calibrator mode is selected (see :CALibrate:CALibrator:MODE), this command specifies the frequency of the signal in Hz.