:CALibrate:CALibrator:MODE

Command Syntax

:CALibrate:CALibrator:MODE {DC | PCOMp | PCNDc | TOUT | ZERO | ONE | PPOSitive | PNSingle
   | PNEGative | PNSingle | FSYNth | TCLock | DCLock | CSERdes | OMHZ | FMHZ | OHMHz}

Query Syntax

:CALibrate:CALibrator:MODE?

Description

This command selects the output mode:

For most of the AC signal output modes, you can use the :CALibrate:CALibrator:AOENable command to enable the output on the AUX OUT connector as well.. DC levels cannot be enabled on the AUX OUT output.

Query Response

{DC | PCOM | PCND | TOUT | ZERO | ONE | PPOS | PNS | PNEG | PNS | FSYN | TCL
   | DCL | CSER | OMHZ | FMHZ | OHMH}