:CALibrate:CALibrator:DCOFfset

Command Syntax

:CALibrate:CALibrator:DCOFfset  <voltage>

<voltage> is a double.

Query Syntax

:CALibrate:CALibrator:DCOFfset?

Description

When the DC level calibrator mode is selected (see :CALibrate:CALibrator:MODE), this command sets the DC voltage output on the oscilloscope's front-panel calibration output (Cal Out). This output can be used to:

  • Manually verify the DC accuracy of a instrument's electrical channel calibration.
  • Calibrate a probe.