:CALibrate:CALibrator:PWIDth

Command Syntax

:CALibrate:CALibrator:PWIDth  <time>

<time> is a double.

Query Syntax

:CALibrate:CALibrator:PWIDth?

Description

When the Pulse Positive, Pulse Positive Single, Pulse Negative, or Pulse Negative Single calibrator mode is selected (see :CALibrate:CALibrator:MODE), this command specifies the width of the pulse.