:CHANnel:YBOTtom?
Query Syntax
:CHANnelN:YBOTtom?
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Description
Queries the amplitude value represented by the graticule's bottom edge. To query the amplitude value represented by the graticule's top edge, use :CHANnel:YTOP?. Use the :CHANnel:YSCale command to set the amplitude scale value in volts or Watts. Use the :CHANnel:YOFFset command to set the amplitude offset.