:CHANnel:YOFFset
Command Syntax
:CHANnelN:YOFFset <offset>
<offset> is a double.
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:YOFFset?
Description
Sets the voltage (or Watts) value that is represented at the center of the display for electrical channels and the second graticule division from the bottom of the display screen for optical channels. Offset parameters are vertical scale dependent. Use the :CHANnel:YSCale command to change a channel's vertical scale. The waveform's offset value represents an absolute value on the display.