:CHANnel:YSCale:FINE
Command Syntax
:CHANnelN:YSCale:FINE {{OFF | 0} | {ON | 1}}
Where N identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:CHANnelN:YSCale:FINE?
Query Response
{0 | 1}
Description
Enables or disables fine adjustment of the vertical scale.
When OFF (coarse adjustment), the vertical scale is adjusted in a 1-2-5 sequence.
When ON (fine adjustment), the vertical scale is adjusted in smaller, evenly spaced increments.