:CMODe:EYE:CWINdow
Command Syntax
:CMODeN:EYE:CWINdow TIME{1:4}
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
Query Syntax
:CMODeN:EYE:CWINdow?
Description
The :CMODe:EYE:CWINdow command allows you to assign a common-mode real-time eye waveform to a Waveform content window.
In Infiniium, several different types of content windows exist. Common-mode channel waveforms can only be displayed in a Waveform (TIME) content window of which there is currently only one available.
| Argument | Displayed Waveform Content Window |
Number of Available Windows |
Scale Units | |
|---|---|---|---|---|
| Programmatically | Via Front Panel |
|||
| TIME{1:4} | Waveform | 4 | 4 | Y-Axis: Volts or Watts (linear scale) X-Axis: seconds |