:CMODe:EYE:WINDow:TRACking

Command Syntax

:CMODeN:EYE:WINDow:TRACking  {{ON | 1} | {OFF | 0}}

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

Query Syntax

:CMODeN:EYE:WINDow:TRACking?

Query Response

{1 | 0}

Description

Specifies whether a signal tracks the global eye window definition or uses its own eye window definition.

The global eye window definition is set using the :MEASure:EYE:WINDow commands (see Eye Window Configuration Commands).

Example Command Sequence

:CMODe1:EYE:WINDow:TRACking OFF
:CMODe1:EYE:WINDow:METHod EOPening
:CMODe1:EYE:WINDow:LEFT 40.0
:CMODe1:EYE:WINDow:RIGHt 60.0