:CMODe:EYE:UUNits
Command Syntax
:CMODeN:EYE:UUNits {UINTerval | SECond}
Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.
Query Syntax
:CMODeN:EYE:UUNits?
Query Response
{UINT | SEC}
Description
This command specifies the user interface's units option for the real-time eye horizontal Scale and Position controls. You can select either Unit Intervals (UIs) or time (in seconds).
To specify the real-time eye horizontal scale and position in terms of UI units, use the :CMODe:EYE:UIXRange and :CMODe:EYE:UIXPosition commands.
To specify the real-time eye horizontal scale and position in terms of time units, use the :CMODe:EYE:XSCale and :CMODe:EYE:XPOSition commands.