:CMODe:EYE:UIXPosition

Command Syntax

:CMODeN:EYE:UIXPosition <time_in_UI>
            

Where N identifies a specific common-mode waveform in the form "<connection1-8>_<ch1|ch3|ch5|ch7>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1|ch3|ch5|ch7>". When two channels are paired to create a differential waveform and a common-mode waveform, the odd-numbered channel is used when specifying the waveform. For example, connection 5 common-mode waveform 3 (from the pairing of channels 3 and 4) is CMODe5_3.

<time_in_UI> is a double in UI (unit interval) units.

Query Syntax

:CMODeN:EYE:UIXPosition?

Description

Sets the common-mode waveform N horizontal time position (center display location) of the real-time eye display in UI units.

This command directly affects the real-time eye's horizontal position setting in seconds (see the :CMODe:EYE:XPOSition command).

To set the horizontal time range of the real-time eye display in UI units, use the :CMODe:EYE:UIXRange command.