:DISK:SIMage:IMETadata

Command Syntax

:DISK:SIMage:IMETadata {ON | OFF}

Query Syntax

:DISK:SIMage:IMETadata?

Description

Turns on and off the inclusion of metadata when saving a screen image file using the :DISK:SIMage:SAVE command. Saving metadata only applies to screen captures that are saved as jpg or tiff files. To view or edit the metadata placed in your screen image file, you can right click on the file in Window's File Explorer and from the shortcut menu select Properties. In the Properties dialog box, click the Details tab as shown in this picture. To edit the metadata fields for your image, click on the Value entree shown on the dialog box. The following table lists the metadata fields that Infiniium populates. The query form of the command returns the current setting.

Metadata Added to Screen Captures
Metadata Field Value Examples
Subject Screen Capture
Comments D9300A (S/N USXXXXXXXX)
Instruments:
Connection 1 Instrument
(MYXXXXXXXX)
Date taken 10/23/2020 4:32 PM
Program name Infiniium 2026 (A.0X.XX.XXX)
Camera maker Keysight Technologies
Camera model Infiniium 2026 (A.0X.XX.XXX)
Name ScreenCapture.jpg