:DISK:SIMage:INVert

Command Syntax

:DISK:SIMage:INVert {ON | OFF}

Query Syntax

:DISK:SIMage:INVert?

Query Response

{1 | 0}

Description

Turns on and off the inversion the graticule area's background color on a saved image file. When on, an inverted image will be captured and saved into a file by the :DISK:SIMage:SAVE command. The entire application window is saved with the graticule black upon a white background. The waveform colors remain unchanged. When printing a hard copy of the waveform, combine this command with the :DISK:SIMage:WINDow command (graticule only) to save ink or toner.