:DISK:SIMage:MONochrome

Command Syntax

:DISK:SIMage:MONochrome {ON | OFF | 1 | 0}

Query Syntax

:DISK:SIMage:MONochrome?

Query Response

{1 | 0}

Description

Turns monochrome screen capture on and off when using the :DISK:SIMage:SAVE command. When on, a black and white image will be captured and saved into a file by the :DISK:SIMage:FNAMe command. Selecting monochrome automatically inverts the graticule area's background color.