:DISK:SIMage:SINClude
Command Syntax
:DISK:SIMage:SINClude {CHANnel{N} | FUNCtion{1:64} | WMEMory{1:8} | CGMemroy{1:8}}
{N} identifies a specific channel in the form "<connection1-8>_<ch1-8>". With connection 1, the connection number part (that is, "1_") is optional, and you can simply use the channel number "<ch1-8>". For example, connection 4 channel 2 is CHANnel4_2.
Query Syntax
:DISK:SIMage:SINClude?
Description
Selects one and only one of any displayed waveforms to be included when saving a screen image using the :DISK:SIMage:SAVE command. By default, all waveforms visible on the display are saved in the screen capture. However, when you select one waveform using this command, all other waveform's will be hidden except for their ground marker (
), which are shown on the screen's right side. Including these markers serves as a reminder that other waveforms were present on the display.