:DISK:SIMage:WINDow
Command Syntax
:DISK:SIMage:WINDow {DISPlay | TIME1 | SHERtz{1:4} | DBHertz{1:4} | DHERtz{1:4}}
Query Syntax
:DISK:SIMage:WINDow?
Description
Selects to save the entire display, including items such as menu bar and toolbars when using the :DISK:SIMage:SAVE command. Or, a specific waveform content window: Waveform, Decibels (Hz), Degrees (Hz), or Seconds (Hz). If a waveform content window is selected, use :DISK:SIMage:SINClude to select the which content window waveforms to include in the screen capture. Any dialog boxes open and positioned over the viewing area are not saved in the file.
| Argument | Displayed Waveform Content Window |
|---|---|
| DISPlay | The entire display including the currently displayed waveform content window. |
| TIME{1} | Waveform |
| SHERtz{1:4} | Seconds (Hz) |
| DBHertz{1:4} | Decibels (Hz) |
| DHERtz{1:4} | Degrees (Hz) |