:DISK:WAVeform:LINTerpolate

Command Syntax

:DISK:WAVeform:LINTerpolate {ON | OFF | 1 | 0}

Query Syntax

:DISK:WAVeform:LINTerpolate?

Query Response

 {ON | OFF | 1 | 0}

Description

Turns on linear interpolation to make the Y-values equally spaced in the saved waveform file. Linear interpolation is available for the following data formats as selected with the :DISK:WAVeform:SAVE:FTYPe command:

  • Waveform Files, Y values (WYValues)
  • Waveform Files, XY values (WXYValues)