:DISK:WAVeform:SAVE:SOURce

Command Syntax

:DISK:WAVeform:SAVE:SOURce <source_waveform>

Where <source_waveform> can be one of the following:

  • CHANnel<connection1-8>_<ch1-8>; With connection 1, the "1_" part is optional, and you can simply use CHANnel<ch1-8>.
  • DIFF{1:4}
  • CGMemory{1:8}
  • FUNCtion{1:64}

Query Syntax

:DISK:WAVeform:SAVE:SOURce?

Description

Selects the source waveform for saving to a waveform file. Use :DISK:WAVeform:SAVE to actually save the file.

Parent Command