:DISK:WAVeform:SAVE:SALL

Command Syntax

:DISK:WAVeform:SAVE:SALL {ON | OFF | 1 | 0}

Query Syntax

:DISK:WAVeform:SAVE:SALL?

Query Response

 {ON | OFF | 1 | 0}

Description

When saving BIN (.bin) format files (see :DISK:WAVeform:SAVE:FTYPe), this command enables or disables Save All Waveforms. When on, all waveforms are saved to the .bin file instead of just the selected signal.

Some post-processing programs require multiple waveforms in one BIN (.bin) format file.