:DISK:WAVeform:SAVE
Command Syntax
:DISK:WAVeform:SAVE
Description
Saves a single-valued waveform to a file. Use the :DISK:WAVeform:FNAMe command to specify the file name. Use the :DISK:WAVeform:SAVE:FTYPe command to specify the waveform file type.
Specify the source waveform that you want to save using the :DISK:WAVeform:SAVE:SOURce command. To increment the automatic file number index, use the :DISK:WAVeform:FNAMe:AUPDate command.
To load a waveform file into one of Infiniium's eight color grade memories, use the :WMEMory:FILE:LOAD and :WMEMory:FILE:NAME commands.
Related Commands
:DISK:WAVeform:FNAMefile name for saving a waveform.:DISK:WAVeform:FNAMe:AUPDateincrements a file name's autonumber.:DISK:WAVeform:FNAMe:USTandardresets to standard file name.:DISK:WAVeform:LINTerpolateselects linear interpolation of Y values in file.:DISK:WAVeform:SAVE:FTYPeselects file format.:DISK:WAVeform:REGionspecifies whether all data or just the on-screen data is to be saved.:DISK:WAVeform:SAVE:SOURcespecifies source waveform.
Example Command Sequence
:DISK:WAVeform:SAVE:SOURce CHAN1_1 :DISK:WAVeform:SAVE:FTYPe HDF5 :DISK:WAVeform:FNAMe "%USER_DATA_DIR%\Waveforms\myfile" :DISK:WAVeform:SAVE;*OPC?