:DISPlay:WINDow:DBHertz{N}:LEGend:EXPand
Command Syntax
:DISPlay:WINDow:DBHertz{N}:LEGend:EXPand {ON | OFF}
{N} identifies a widow {1:4}.
Query Syntax
:DISPlay:WINDow:DBHertz{N}:LEGend:EXPand?
Description
Expands or contracts the Signals legend that is shown in the Decibels (Hz) waveform content window. The legend shows:
- Any output waveforms of the FFT function (FFT command) (when defined as magnitude).
To completely remove the signal legend from all frequency-domain windows, use the :DISPlay:WINDow:FDLegend command.