:DISPlay:WINDow:DBHertz{N}:TOPMost
Command Syntax
:DISPlay:WINDow:DBHertz{N}:TOPMost {FUNCtion{1:64} | TRACe{1:128} }
{N} identifies a widow {1:4}.
Query Syntax
:DISPlay:WINDow:DBHertz{1:4}:TOPMost?
Description
When a Decibels (Hz) waveform content window is displayed in tab tiled mode and there are multiple displayed waveforms, selects a waveform to display in the graticule area. The output of the FFT function (FFT command) can be defined as magnitude.