:DISPlay:WINDow:DBHertz{N}:LOCation
Command Syntax
:DISPlay:WINDow:DBHertzN:LOCation {A1 | A2 | A3 | A4
| B1 | B2 | B3 | B4
| C1 | C2 | C3 | C4
| D1 | D2 | D3 | D4 | FLOat | MAXimize | MINimize}
Where N indicates one of 4 possible Decibels (Hz) windows. For example, DBHertz2.
Query Syntax
:DISPlay:WINDow:DBHertzN:LOCation?
Query Response
{A1 | A2 | A3 | A4
| B1 | B2 | B3 | B4
| C1 | C2 | C3 | C4
| D1 | D2 | D3 | D4 | FLO | MAX | MIN}
Description
Selects the location to display a Decibels (Hz) waveform content window. Use the arguments listed below to specify the position.
| A1 | A2 | A3 | A4 |
| B1 | B2 | B3 | B4 |
| C1 | C2 | C3 | C4 |
| D1 | D2 | D3 | D4 |
- FLOat
- The content window is undocked (floated) from Infiniium's window. To re-dock the window, resend the command using the
A1,A2,A3,A4,B1,B2,B3,B4,C1,C2,C3,C4,D1,D2,D3, orD4arguments. - MAXimize
- The content window occupies the space of all nine panel locations.
- MINimize
- The content window is lowered to a task bar.
Example Command Sequence
:DISPlay:WINDow:DBHertz2:LOCation C3