:DISPlay:WINDow:DHERtz{N}:LEGend:EXPand

Command Syntax

:DISPlay:WINDow:DHERtz{N}:LEGend:EXPand {ON | OFF}

{N} identifies a widow {1:4}.

Query Syntax

:DISPlay:WINDow:DHERtz{N}:LEGend:EXPand?

Description

Expands or contracts the Signals legend that is shown in the Degrees (Hz) waveform content window. The legend identifies:

  • Any output waveforms of the FFT function (FFT command) (when defined as phase).

To completely remove the signal legend from all frequency-domain windows, use the :DISPlay:WINDow:FDLegend command.

Sibling Commands