:DISPlay:WINDow:DHERtz{N}:TOPMost

Command Syntax

:DISPlay:WINDow:DHERtz{N}:TOPMost  {FUNCtion{1:64} | TRACe{1:128} }

{N} identifies a widow {1:4}.

Query Syntax

:DISPlay:WINDow:DHERtz{1:4}:TOPMost?

Description

When a Degrees (Hz) waveform content window is displayed in tab tiled mode and there are multiple displayed waveforms, selects a waveform to display in the graticule area. The output of the FFT function (FFT command) can be defined as phase.

Sibling Commands