:DISPlay:WINDow:DHERtz{N}:LOCation

Command Syntax

:DISPlay:WINDow:DHERtzN:LOCation {A1 | A2 | A3 | A4 
   | B1 | B2 | B3 | B4 
   | C1 | C2 | C3 | C4 
   | D1 | D2 | D3 | D4 | FLOat | MAXimize | MINimize}

Where N indicates one of 4 possible Degrees (Hz) windows. For example, DHERtz2.

Query Syntax

:DISPlay:WINDow:DHERtzN:LOCation?

Query Response

{A1 | A2 | A3 | A4 
   | B1 | B2 | B3 | B4 
   | C1 | C2 | C3 | C4 
   | D1 | D2 | D3 | D4 | FLO | MAX | MIN}

Description

Selects the location to display a Degrees (Hz) waveform content window. Use the arguments listed below to specify the position.

Display Panel Locations
A1 A2 A3 A4
B1 B2 B3 B4
C1 C2 C3 C4
D1 D2 D3 D4

FLOat
The content window is undocked (floated) from Infiniium's window. To re-dock the window, resend the command using the A1, A2, A3, A4, B1, B2, B3, B4, C1, C2, C3, C4, D1, D2, D3, or D4 arguments.
MAXimize
The content window occupies the space of all nine panel locations.
MINimize
The content window is lowered to a task bar.

Example Command Sequence

:DISPlay:WINDow:DHERtz2:LOCation C3

Sibling Commands