:FUNCtion:PARameters:DEConvolve:ALIGn

Command Syntax

:FUNCtionN:PARameters:DEConvolve:ALIGn {ON | OFF | 1 | 0}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtion{1:64}:PARameters:DEConvolve:ALIGn?

Query Response

{1 | 0}

Description

For an Remove s2p operator (:FUNCtion:FOPerator), turns on and off the waveform alignment between the operator's input and output waveforms. Turning off this setting allows you to view any delay introduced by the DUT. By default, this setting is on and the waveforms are aligned.