:FUNCtion:PARameters:DEConvolve:BSPan?
Query Syntax
:FUNCtionN:PARameters:DEConvolve:BSPan?
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Response
<frequency_span> is a double.
Description
When the BANDpass filter type is selected (see :FUNCtion:PARameters:DEConvolve:BLIMit), this query returns the span of the bandpass filter.