:FUNCtion:PARameters:DEConvolve:BANDwidth:AUTO

Command Syntax

:FUNCtionN:PARameters:DEConvolve:BANDwidth:AUTO {ON | OFF | 1 | 0}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:DEConvolve:BANDwidth:AUTO?

Query Response

{1 | 0}

Description

Turns on or off automatic bandwidth setting for a Remove s2p operator (:FUNCtion:FOPerator). When off, use the parent command (:FUNCtion:PARameters:DEConvolve:BANDwidth) to enter the bandwidth.

Example Command Sequence

:FUNCtion2:FOPerator DEConvolve
:FUNCtion2:PARameters:DEConvolve:FNAMe "C:\Users<user_name>\Documents\Keysight\Infiniium\S-Parameter Data\DUT_4.s2p"
:FUNCtion2:PARameters:DEConvolve:FMODel ON  // Flips  S-parameters ports
:FUNCtion2:PARameters:DEConvolve:BANDwidth:AUTO OFF
:FUNCtion2:PARameters:DEConvolve:BLIMit GAUSsian
:FUNCtion2:PARameters:DEConvolve:BANDwidth 7.5E9
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
*OPC?
…  //  Your code to synchronize execution timing.

Parent Command