:FUNCtion:PARameters:DEConvolve:FRELoad

Command Syntax

:FUNCtionN:PARameters:DEConvolve:FRELoad

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Description

Reloads an S-parameter file for a Remove s2p operator (:FUNCtion:FOPerator). The file must have been previously loaded using the :FUNCtion:PARameters:DEConvolve:FNAMe command.

Example Command Sequence

:FUNCtion2:FOPerator DEConvolve
:FUNCtion2:PARameters:DEConvolve:FNAMe "C:\Users<user_name>\Documents\Keysight\Infiniium\S-Parameter Data\DUT_4.s2p"
:FUNCtion2:PARameters:DEConvolve:FMODel ON  // Flips  S-parameters ports
:FUNCtion2:COLor TCOLor4
:FUNCtion2:DISPlay ON
……
:FUNCtion2:PARameters:DEConvolve:FRELoad