:FUNCtion:PARameters:USER:COMMents?
Query Syntax
:FUNCtionN:PARameters:USER:COMMents?
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Description
Returns the comment string for the selected user-defined operator (USER Argument). The comment string is defined in the operator's XML definition file using the <Comments> tag.
Use the :FUNCtion:PARameters:USER:CFILe sibling command to configure the function.