:FUNCtion:PARameters:USER:LSTatus:DETails?
Query Syntax
:FUNCtionN:PARameters:USER:LSTatus:DETails?
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Description
If the status of the configuration file load is questionable or invalid (see :FUNCtion:PARameters:USER:LSTatus?), this query returns a string that may provide additional details.
If the status of the configuration file load is valid, this query returns an empty string.
For a basic reason for the questionable or invalid status, use the :FUNCtion:PARameters:USER:LSTatus:REASon? sibling query.
Use the :FUNCtion:PARameters:USER:CFILe command to configure the function.