:FUNCtion:PARameters:USER:CONTrol:STRing

Command Syntax

:FUNCtionN:PARameters:USER:CONTrol{1:4}:STRing

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:FUNCtionN:PARameters:USER:CONTrol{1:4}:STRing?

Description

Sets the value of a function's user-defined control which has been configured as a string. User-defined controls are shown in the function's User Operator Setup dialog box. The controls are numbered 1 through 4 starting with the top control shown in the dialog box. For example, the following figure shows how four controls are numbered:

  • "N", an integer, is control 1.
  • "Fc", a double, is control 2.
  • "Test String", a string, is control 3.
  • "Selections", a drop-down list (enumeration), is control 4.

Since control 3 is defined as a string, you could set its value to "A string!" using the following command:

:FUNCtion1:PARameters:USER:CONTrol3:STRing "A string!"

In this case, the sibling commands DOUBle, ENUM, FILE, and INTeger do not affect this user-defined control as the control has been defined as an string in the XML configuration file. This user-defined control is defined by the XML file's <String> element. The query form of the command returns current value of the user-defined control.

Use the :FUNCtion:PARameters:USER:CFILe command to load the XML configuration file for the function.